Technical FAQs

Ask a Question

Why does StruxureWare Data Center Expert not have firmware updates available within the Firmware Update window after check for updates?

Issue:

Why does StruxureWare Data Center Expert not have firmware updates available within the Firmware Update window after check for updates?

Product Line:

StruxureWare Data Center Expert StruxureWare Central

Environment:

StruxureWare Data Center Expert all versions

Cause:

A key feature within Data Center Expert is the ability mass to update the firmware of APC devices. This feature is dependent on the latest firmware version available loaded on the Data Center Expert server. The Expert server relies on FTP and HTTPS to both navigate to and download the latest available catalog files.

Resolution:

Data Center Expert reaches out to updates.apc.com to obtain the latest available firmware. Using HTTPS to navigate to the URL and then FTP to download the catalog file. In most cases the reason that Data Center Expert doesn't have the firmwares available is because one or both protocols are being blocked. Generally, opening or adding an exception to a firewall allowing the Data Center Expert server to reach the web corrects this issue.
 
Was this helpful?
What can we do to improve the information ?