Technical FAQs

Ask a Question

What accessories are available for AR3100X717 or AR3104X717?

Customer is in need of accessories for AR3100X717 or AR3104X717.

Product Line:
NetShelter Dell OEM

All versions and serial ranges.

Need to identify compatible accessories.

All accessories that are compatible with AR3100 and AR3104 also compatible with AR3100X717 and AR3104X717 with one exception AR7719, Castor Kit. For a list of the available accessories please see the NetShelter Accessory Compatibility Chart which is available from the Knowledge Base on the APC website. Please search for document FA158651: 

Was this helpful?
What can we do to improve the information ?