Technical FAQs

Ask a Question

How to Display firmware identification number on an EcoBreeze Expansion Module.

                                                                                                                                                           

Issue:   
How to Display firmware identification number on an EcoBreeze Expansion Module

Product line:
ACEC200, ACEC201 

Environment:  
All serial numbers 

Cause:  
Install 

Resolution:    

On switch-on, during the start-up test phase, holding the DOWN button, the project identification is displayed for about 2 seconds. The information regarding the

versions/revisions of the project is displayed in sequence. The procedure is exited automatically at the end of the start-up.

 

Was this helpful?
What can we do to improve the information ?