Technical FAQs
Technical FAQs
Issue:
Temperature/Humidity Sensor Duplicate CAN Address
Product line:
ACDA901
Environment:
All Serial Numbers
Cause:
Two or more AP9520TH sensors have the same CAN address
Resolution:
This alarm occurs if you have sensors on the a-link chain with the same id address. Please see chart below on how to set the ID a-link address. .