Technical FAQs

Ask a Question

How to Load VMware vSphere Client onto a PC

Issue:
How to Load VMware vSphere Client onto a PC

Product Line:
VMware vSphere Client

Environment:
Microsoft Windows XP, Vista, Win 7, Win8, Win8.1, Win 10
NOTE: vSphere Client requires .Net Framework 3.5 be present before it will install properly. Windows XP, 8.x, and 10.x do not ship with .Net Framework 3.5 so it must be installed prior to installing vSphere client. See Microsoft forum post http://answers.microsoft.com/en-us/windows/forum/windows8_1_pr-networking/when-installing-the-vmware-vsphere-51-client-i-get/8cfa9152-fb46-432e-99f3-3ba3558f3845 for more information.

Cause:
Informational

Solution:

Please review the attached PDF.
Was this helpful?
What can we do to improve the information ?