Technical FAQs

Ask a Question

What are the differences between the NetShelter SX cabinets and the NetShelter SX Networking cabinets?

Issue:
Customers need to know the differences between the NetShelter SX and the NetShelter SX Networking cabinets. 

Product Line:
NetShelter SX
 
Environment:

All versions and serial ranges.
 
Cause:
The NetShelter SX and the NetShelter SX Networking cabinets have different features.
 
Resolution:
see attached file.
Was this helpful?
What can we do to improve the information ?