Technical FAQs

Ask a Question

Serial devices on a Netbots connected to the same port as a camera pod can cause bot to reboot.

Issue:

Serial devices on a Netbots connected to the same port as a camera pod can cause bot to reboot.

Product Line:

NetBotz

Environment:

All versions

Cause:

RS232-based Serial Devices connected to a USB-to-Serial Port adapter and USB modems should not share the same USB port or hub as a Camera Pod 120, Camera Pod 160, or a CCTV Pod 120. Doing so may cause configured USB-based Serial devices to disappear and then reappear, or your appliance may unexpectedly restart

Resolution:

Make sure these devices use different ports or hubs.

Was this helpful?
What can we do to improve the information ?