Details Returned from MIB2 UPS Devices via Netbotz Advanced Device Crawlers
Issue:
Details Returned from MIB2 UPS Devices via Netbotz Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for MIB2 UPS systems assuming the MIB2-UPS DDF (Device Definition File) is installed on the NetBotz appliance and the MIB2 UPS is SNMP enabled. Please note that not all information listed below is available on all MIB2 UPS models.
Resolution:
Vendor
Description
Battery Status
Time On Battery
Battery Run Time Remaining
Remaining Battery Capacity
Battery Voltage
Battery Current
Battery Temperature
Input Line Voltage
Input Line Current
Input Line True Power
Output Source
Output Frequency
Output Line Current
Output Line True Power
Output Line Current Load
Bypass Frequency
Bypass Line Current
Bypass Line True Power
* APC UPS units with some network card firmwares do not work with the standard MIB2 UPS OIDs. Netbotz does have an APC specific DDF file that does return this information on most UPS units.