Technical FAQs

Ask a Question

Why isn't my DNS change saving in StruxureWare Data Center Expert?

Issue:

Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes.

Product Line:

StruxureWare Data Center Expert

Environment:

StruxureWare Data Center Expert VM with single NIC configured

Cause:

It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.

Resolution:

This issue does not occur when using SSH or a direct keyboard connection and the apcsetup configuration user.

This issue is slated to be resolved in DCE version 7.2.6
 
Was this helpful?
What can we do to improve the information ?