Why does the NetBotz wireless device LED stay red.
Issue:
NetBotz wireless device LED stays red.
Product Line:
NetBotz version 3
Environment:
NetBotz wireless sensors / pods NBSP180
Cause:
When you do a long reset button push the led goes red after 10s of holding the button in and if the button is physically stuck in the red led will stay on. This could also happen with a single push of the reset button.
Resolution:
You can clear the LED by freeing the button. To free the buton, move it around or side to side using a pin or paper clip.