Adding an Extension Cable or Hub to a Previously Recognized USB-to-Serial-Port Adapter causes serial device to be reconfigured.
Issue:
Adding an Extension Cable or Hub to a Previously Recognized USB-to-Serial-Port Adapter causes serial device to be reconfigured.
Product Line:
NetBotz
Environment:
NetBotz and RS232 sensor connections using USB
Cause:
If you add an extension cable or hub between the appliance and a
USB-to-Serial-Port adapter or hub after the USB-to-Serial-Port adapter
or hub has been connected to your appliance, all of the serial ports on
the converter are recognized as new ports by the appliance.
Resolution:
If you
previously configured serial devices on these ports, use the Serial
Devices task to reconfigure these devices.