Technical FAQs

Ask a Question

User Access Levels for Version 1 Netbotz Appliances


User Access Levels for Version 1 Netbotz Appliances

Product Line:



NetBotz version 1


Configuration options


User Access Levels for Version 1 Appliances

The Netbotz 300, 303, 310, 400 series appliances have 3 levels of access:

Sensor Access -lets you view camera image and sensor readings only.

Application Access -gives Sensor Access plus ability to view information from any licensed applications (Device Crawlers, Advanced Device Crawlers, or Branch Checker).

Supervisor Access- provides all of the capabilities of the two previous levels plus the ability to change configuration settings and thresholds.

Each access level can be secured with a userid and password.

The user id's and passwords are not transmitted encrypted.

These appliances does not support SSL. If there is a requirement to prevent viewing beyond the user id/pswd security described, it would need to be done through access control with a router or firewall.

Was this helpful?
What can we do to improve the information ?