Technical FAQs

Ask a Question

Polarity of 0-5V Sensor Cable NBCD0001

Issue:

Polarity of 0-5V Sensor Cable NBCD0001

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2
NBCD0001

Cause:

Configuation / connection to 0-5v source.

Resolution:

One end of NetBotz 0-5V Sensor Cable is DIN6 (ps/2) connector, which goes to an external sensor port on 320/420/500 model or Sensor Pod 120. On the other end are 2 wires - the black wire is ground (-); the red is sense (+).

Was this helpful?
What can we do to improve the information ?