Technical FAQs

Ask a Question

Network Management Card Event Configuration Config.ini Syntax


Issue

Need assistance understanding the config.ini syntax relating to the [EventActionConfig] or [DeviceControlPolicyConfig] sections.


Product Line
  • Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (AP9320, AP9340, Netbotz 200)
 
  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.

 


Environment
 
  • All serial numbers
  • Users working with config.ini and event notifications/device control policy
  • v3.X.X, v5.X.X, v6.X.X firmware

     
Cause

The syntax is provided for general information and understanding of the config.ini sections noted.


Resolution

Refer to the attached PDF supplement.

 
 
Was this helpful?
What can we do to improve the information ?