Do the 800 mm wide NetShelter SV cabinets have 1U rackmount spaces in the vertical mounting rails?
Issue:
This space would be perfect to mount small IT devices into.
Product Line:
NetShelter SV
Environment:
800 mm width only, all serial numbers.
Cause:
It appears there may be a 1U punch out in the vertical mounting rails.
Resolution:
Yes, all of the NetShelter SV 800 mm wide cabinets have EIA 1U punch outs with square mounting holes. These spaces can be used to mount small IT devices, cable management, PDU...etc.