Technical FAQs

Ask a Question

What is the input voltage required for the InRow ACRD?

Issue:
What is the input voltage required for the InRow ACRD? 
 
Product line:
ACRD100, ACRD101, ACRD200, ACRD201
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
The InRow ACRD unit uses a single phase 208V/60Hz input in NAM and a 230V/50Hz input in the rest of the world.
Was this helpful?
What can we do to improve the information ?