Technical FAQs

Ask a Question

Why does my Symmetra PX UPS show a power module status of NA when first installed?

Symmetra PX UPS shows power module status as "NA" within the Network Management Card interface when the module is first installed

Product Line
  • Symmetra PX
  • UPS Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
  • UPS Network Management Card 2 (NMC2) - AP9630/30CH, AP9631/31CH

  • All UPS firmware revisions
  • All NMC1 and NMC2 firmware revisions


Still under investigation

Perform a reboot on the NMC management interface. In order to do this, access the web interface and navigate to the Administration tab->General->Reset/Reboot and select "Reboot management interface." Press apply.

If caller is at the UPS they can also press and release the pin hole reset button to accomplish the same reset.
Was this helpful?
What can we do to improve the information ?