NetBotz Room Monitor 355/455 POE Power Specifications
Issue:
NetBotz Room Monitor 355/455 POE Power Specifications
Product Line:
NetBotz
Environment:
NetBotz Version 3 using POE
Cause:
POE specifications
Resolution:
The NetBotz 355 and 455 are Class 0 POE devices.
The IEEE standard 802.3 for supplying power over Ethernet allows the device providing power to use a voltage between 36–57 V DC. The nominal voltage is 48 V with a current of 10–400 mA, subject to a maximum load power of 15.40 Watts.