Technical FAQs

Ask a Question

What is the accuracy level of the AP9512TBLK and AP9512THBLK environmental sensors?


Issue

What is the accuracy level of the AP9512TBLK and AP9512THBLK environmental sensors?


Product Line
  • Environmental Monitoring
    • AP9512T/TBLK
    • AP9512TH/THBLK


Environment
  • All serial numbers


Cause

General reference information


Resolution


Below you will find the accuracy ratings of the AP9512TBLK and AP9512THBLK sensors.


Temperature accuracy:

±2º C (±3º F ), from 0 to 40º C (32 to 104º F)



Humidity accuracy:

±8 % RH, 10 to 90% RH, at 25º C (77º F)
±8 % RH, 30 to 80% RH, from 15 to 30 º C (59 to 95º F)



Probe operating temperature:

0 to 60º C (32 to 140º F)


User input response time:

200 mS
 

Was this helpful?
What can we do to improve the information ?