Technical FAQs

Ask a Question

What are the BTU/hr rating for NetBotz appliances?

Issue:

What are the BTU/hr rating for NetBotz appliances?

Product Line:

Netbotz Appliance

Environment:

Netbotz Appliance Version

Cause:

When building a data center, cooling is a key factor to maintain proper operational temperatures. This article contains the BTU/hr rating for NetBotz appliances.

Resolution:

The information below contains calculations for a fully populated NetBotz Appliance

NetBotz Rackmonitor 200/450/550/570
Part Number NBRK0200, NBRK0450, NBRK0550, NBRK0570
Max Power Draw = 45.1W
BTU/hr = 153.88

NetBotz Wallmonitor 355/455
Part Number NBWL0355, NBWL0455
Max Power Draw = 12.0W
BTU/hr = 40.94

The following formula was used to calculate BTU/hr
P(BTU/hr) = 3.412141633 × P(W)
Was this helpful?
What can we do to improve the information ?