How to check the model and serial number of an ACRP100
Issue: How to check the model and serial number of an ACRP100
Product line: ACRP100
Environment: All serial numbers
Cause: To help tech support identify the unit and its warranty status
Resolution:
Press the < ESC> button until you get to the “ON/STANDBY” screen. Then use the down arrow to scroll though the display. When you get to the screen “ABOUT INROW” stop and make sure the arrow on the left side of the display is pointing at it and the hit the <ENTER/RETURN> button.