Technical FAQs

Ask a Question

Can the 0U accessory mounting brackets be installed into the front of a NetShelter SV?

Issue:
Customers may want to install the 0U accessory mounting brackets into the front of a NetShelter SV cabinet.

Product Line:
NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The owner's manual shows the 0U accessory mounting brackets installed into the rear of the NetShelter SV cabinet.

Resolution:
The 0U accessory mounting brackets can only be installed into the rear of the NetShelter SV cabinet.
Was this helpful?
What can we do to improve the information ?