Technical FAQs

Ask a Question

What are the technical specifications of AR3100X717 or AR3104X717: height, width, depth, load ratings?

Issue:
Technical specifications are being requested: 

Product Line:
NetShelter Dell OEM

Environment:
All versions and serial ranges

Cause:
Customer requests technical specifications.

Resolution:
Technical specifications are available from Dell. For further support contact APC: www.APC.com/support/contact
AR3100X717 = Dell Part # A7545497
AR3104X717 = Dell Part # A7545498

Was this helpful?
What can we do to improve the information ?