Technical FAQs

Ask a Question

Can the NetShelter CX be deployed in any room or space?

Where can the NetShelter CX be deployed?

Product Line:
NetShelter CX
All versions and serial ranges.
Customers want to make sure that the NetShelter CX is suited for the environment in which they intend to install it.
Optimal performance of these cabinets requires suitably ventilated space or building HVAC system.
The NetShelter CX is not suitable for installation in a small unventilated space.
Was this helpful?
What can we do to improve the information ?