Technical FAQs

Ask a Question

PowerChute Personal Edition v2.1.1 appears in the wrong language

Issue:
PowerChute Personal Edition v2.1.1 appears in the wrong language

Product:
PowerChute Personal Edition

Environment:
All supported Windows OS

Cause:
PowerChute Personal Edition v2.1.1 displays in the language the is set in the Windows Regional Settings


Solution:

PowerChute Personal Edition v2.1.1 displays in the language that is set up in your Windows Regional Settings as long as the language is one of our 8 localizations. For all other languages, PowerChute Personal Edition displays in English. The 8 localized languages are: Japanese, Chinese, Brazilian Portuguese, Russian, German, Italian, Spanish and French.

 

Select the language in Regional Settings that you want the PowerChute Personal Edition user interface (UI) to display. For example, pick English.


The steps mentioned below give Windows XP as example:

1. Go to Start > Settings > Control Panel.


2. Double click on the Regional and Language Options.


3. Click on the Advanced tab.


For example select the English (United States) locale under Language for non-Unicode programs.

 

Was this helpful?
What can we do to improve the information ?