Technical FAQs

Ask a Question

Will the NetShelter SX leveling feet support the full weight of the cabinet and its contents?

Can the full weight of the NetShelter cabinet rest on the leveling feet?
Product Line:
NetShelter SX
All versions and serial ranges.
Customers may want to lift the cabinet off the castors and need reassurance that the leveling feet can bear the full weight of the cabinet and it's contents. (static load rating)
Yes, the leveling feet can support the cabinet up to the rated static load rating of the cabinet.  
Knowledge Base document FA158656 also contains information regarding shipping load, dynamic load and static load ratings.
Was this helpful?
What can we do to improve the information ?