Technical FAQs

Ask a Question

NetBotz location information not retained on Pelco camera after reboot.

Issue:
NetBotz location information not retained on Pelco camera after reboot.

Product Line:
NetBotz
Pelco Cameras

Environment:
Botzware version 4.2 and lower that support Pelco cameras

Cause:
In NetBotz Advanced View, you are able to put specific location information to the NetBotz appliance, all of it's pods, and it's sensors. In the case of a Pelco camera, you can also add the camera to the NetBotz appliance as a shared pod.

We have seen that during a reboot, this location information is not retained for the Pelco camera only. You can re-add this information but it will again be lost on subsequent reboots.

Resolution:
This is  resolved in Botzware version 4.3
 
Was this helpful?
What can we do to improve the information ?