Technical FAQs

Ask a Question

Ports used on NetBotz Appliances

Issue:

Ports used on NetBotz Appliances

Product Line:

NetBotz

Environment:

NetBotz any version

Cause:

Network information / configuration

Resolution:

The following outlines ports used and their application on any NetBotz Version 2 Appliance:

Note: Ports preceded by * can be changed from their default port number.

Incoming:
*Port 80 - HTTP Communication from Advanced View / Basic View / ISX Central
*Port 443 - HTTPS Communication from Advanced View / Basic View / ISX Central
*Port 161, 162 - SNMP Communication from SNMP Manager

Outgoing:
*Port 80 - HTTP Communication to Advanced View / Basic View / ISX Central / HTTP Post to Web Server
*Port 443 - HTTPS Communication to Advanced View / Basic View / ISX Central
*Port 161, 162 - SNMP Communication to SNMP Manager
*Port 25 - SMTP Communication to Email Server
Port 21 - FTP Communication to FTP Server
Port 53 - DNS Communication to DNS Server
Port 2049 - NFS Communication to NAS / SAN
Port 445 - CIFS Communication to NAS / SAN
 
Was this helpful?
What can we do to improve the information ?