Technical FAQs

Ask a Question

Details Returned from MIB2 UPS Devices via Netbotz Advanced Device Crawlers

Issue:

Details Returned from MIB2 UPS Devices via Netbotz Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for MIB2 UPS systems assuming the MIB2-UPS DDF (Device Definition File) is installed on the NetBotz appliance and the MIB2 UPS is SNMP enabled. Please note that not all information listed below is available on all MIB2 UPS models.

Resolution:


  • Vendor
  • Description
  • Battery Status
  • Time On Battery
  • Battery Run Time Remaining
  • Remaining Battery Capacity
  • Battery Voltage
  • Battery Current
  • Battery Temperature
  • Input Line Voltage
  • Input Line Current
  • Input Line True Power
  • Output Source
  • Output Frequency
  • Output Line Current
  • Output Line True Power
  • Output Line Current Load
  • Bypass Frequency
  • Bypass Line Current
  • Bypass Line True Power


* APC UPS units with some network card firmwares do not work with the standard MIB2 UPS OIDs. Netbotz does have an APC specific DDF file that does return this information on most UPS units.
Was this helpful?
What can we do to improve the information ?