KUWAIT - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
KUWAIT - Choose Country or Region
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
Communication Modes for NetBotz Central 2.x
Issue:
Communication Modes for NetBotz Central 2.x
Product Line:
NetBotz Central
Environment:
NetBotz Central version 2.x
Cause:
Communications configurations.
Resolution:
NetBotz Central can communicate with appliances it manages in two different ways:
LAN Mode
Uses port 80 or port 443 (http / https) by default (customizable)
Default mode when appliances are added to NetBotz Central in a normal LAN / network environment
Bi-directional communications between the NetBotz Central and the appliances
NetBotz Central can initiate communications to the appliances
Appliances can initiate communications to the NetBotz Central
Post-only Mode
Uses port 80 or port 443 (http / https) by default (customizable)
Special mode initiated by the appliance for use there is a firewall between the appliance and the
NetBotz Central and only the NetBotz Central has a public IP address (The appliances are protected behind a firewall.)
Uni-directional communications between the appliances and NetBotz Central
Only the appliances initiate communications to the NetBotz Central