Technical FAQs

Ask a Question

NetBotz Central 1.x - End of Sale & End of Support Information

Issue:

NetBotz Central 1.x - End of Sale & End of Support Information

Product Line:

NetBotz Central

Environment:

NetBotz Central version 1.x.

Cause:

NetBotz Central version 1.x was announced as End-of-Sale as of September 3, 2004

Resolution:



This affects all All 1.x versions of NetBotz Central (NBCN1000).

NetBotz will continue to offer technical support for NetBotz Central 1.3 through September 3, 2006. Extended Warranties can be purchased through September 3, 2006. Extended Warranties can NOT be granted past that date. 
Was this helpful?
What can we do to improve the information ?