Technical FAQs

Ask a Question

Does APC support Wake On LAN technology?


Issue

Does APC support Wake On LAN technology?


Product Line

  • All

Environment
  • All


Cause



Background about Wake On LAN technology - t
he computer/machine to be "woken" is shutdown with power reserved for the network card, but not disconnected from its power source. The network card listens for a specific packet containing its MAC address called the "Magic Packet", broadcast on the broadcast address for that particular subnet.


Resolution

Currently, Wake On LAN is not implemented/supported by any APC product.
Was this helpful?
What can we do to improve the information ?