What are the pinouts of the RJ45 sensor connectors on a NetBotz appliance?
Issue: RJ45 Connector Pin Outs For the Netbotz Appliances
Product Line: NetBotz
Environment: NetBotz version 3 sensor cables
Cause: Pin-out specifications.
Resolution:
-NetBotz does not release the pin outs for the RJ45 connectors for any sensors designed for NetBotz Appliances.
-To address this issue, NetBotz sells a standard dry contact cable that is our RJ45 connector one end and two bare dry contact style wires on the other.
-This cable is provided to allow customers to attach our NetBotz Appliances to any dry contact type connection without having to have the RJ45 connector pin outs.