Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
Issue:
The NetShelter cable partition won't install on top of the InRow cooling unit.
Product Line:
NetShelter, InRow Cooling, Row Power Distribution
Environment:
All versions and serial ranges.
Cause:
There are no square holes in the roof of the 300 mm chilled water cooling units so there's nowhere to connect the tabs on the NetShelter cable partition.
Resolution:
Please use ACAC10005 for 300 mm wide applications and ACAC10010 for 600 mm wide applications. Please do not use AR86xx or any other NetShelter cabinet partitions.
A NetShelter trough such as AR8580 or AR8561 may also be used to span the cooling unit but they can not be attached directly to them. NetShelter troughs can span one cabinet width without attaching directly to the cooling unit roof. See the installation manual of the NetShelter trough, instruction #2.
NOTE: The mounting tabs on the bottom of the bottom of the 300 mm wide trough may be bent out of the way if there are no mounting holes.