Technical FAQs

Ask a Question

Pelco camera presets configured on the NetBotz appliance are saved on the camera using a default naming convention

Issue:

Pelco camera presets configured on the NetBotz appliance are saved on the camera using a default naming convention rather than the preset names configured in the NetBotz appliance user interface.

Product Line:

NetBotz, Pelco

Environment:

NetBotz, Pelco

Cause:

This is a known limitation of the integration between the NetBotz appliance and Pelco cameras.

Resolution:

There is no resolution at this time.
 
Was this helpful?
What can we do to improve the information ?