SAINT KITTS AND NEVIS - Choose Country or Region
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
Audio-Video Solutions
AV Power Conditioners with Battery
AV Surge Protectors
AV Power Filters
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
Room Cooling Accessories
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
iBusway for Data Center
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
Room Power Distribution
Cabinet Power Distribution
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
SmartShelter Room
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
Remote Monitoring Services
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
When to replace your battery or UPS
UPS Buying Guide
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
SAINT KITTS AND NEVIS - Choose Country or Region
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
Presets overwritten when more than one NetBotz appliance monitors a Pelco Camera
Issue:
When more than one NetBotz appliance monitors the same Pelco camera, Pelco camera presets can be overwritten.
Product Line:
NetBotz, Pelco
Environment:
NetBotz software Interfaces
Cause:
The NetBotz appliance sets presets using the default pointer on the camera, “Preset 1”.
Users are allowed to discover the same Pelco camera on more than one NetBotz appliance. No warning message is displayed.
Resolution:
Users should not discover the same Pelco camera on more than one NetBotz appliance.