Technical FAQs

Ask a Question

Can split doors be installed on the front of a NetShelter SX, VX or SV cabinet?

Issue: 
It can not be assumed that the rear split doors will install onto the front of the cabinet. Confirmation is needed.  

Product Line: 
NetShelter SX, NetShelter VX, NetShelter SV
 
Environment:
All versions and serial ranges.
 
Cause: 
A customer may want to install split doors onto the front of a NetShelter SX cabinet.
 
Resolution :

Rear split doors can be installed onto the front of a NetShelter SX cabinet. 
A replacement split door kit can be purchased or the existing split rear doors can be swapped to the front of the cabinet.
The replacement door kit includes all of the hardware necessary, including hinges.
Was this helpful?
What can we do to improve the information ?