Export as AVI option in ISX Central not available for Pelco cameras.
Issue:
Export as AVI option in ISX Central not available for Pelco cameras
Product Line:
NetBotz
Pelco cameras
Environment:
Netbotz / Pelco camera integration
Cause:
Due to differences between ISX Central's image options and Pelco camera image options, clips exported using the AVI file type were exporting improperly.
Resolution:
This option may be fixed in a future revision but in ISX Central 5.1, the AVI export option has been removed for Pelco cameras.