Technical FAQs
Technical FAQs
Item Number | Description | Maximum Output Power |
7 | CAN Bus Ports (for Network Port Sharing use only) | 200mA @ 24VDC nominal (4.8 watts) |
8 | USB Port - (for USB drive to upgrade PDU firmware only) | 100mA @ 5VDC nominal |