Cleanable Air Filters Removal and installation
1. Starting with the top air filter, locate the pull tab and pull up and away from filter track.
2. To remove the bottom filter, locate the pull tab and pull down and away from the filter track.
3. Remove dust and debris from the filter media using a vacuum with a soft brush, or rinse the filter media with low pressure water.
4. Inspect the filter for damage or deterioration of the filter media. Make sure the filter is dry before installing.
5. Reinstall the filter.