Technical FAQs

Ask a Question

Upgrade PowerChute Network Shutdown Appliance from version 4.1 to 4.2 and the system web page <ip address:5480> still displays version number 4.1

Issue:
Upgraded PowerChute Network Shutdown Appliance from version 4.1 to 4.2 and the system web page is still displaying version number 4.1

Product Line:
PowerChute Network Shutdown

Environment:
PowerChute Network Shutdown Appliance on VMware ESXi

Cause:
Display name is not updated in /opt/vmware/var/lib/vami/update/data/info/manifest-installed.xml
and
/opt/vmware/share/htdocs/service/core/view-deploy.xml

Solution:
After following the instruction in Schneider Electric FAQ FA276378 to upgrade the PowerChute virtual appliance from version 4.1 to 4.2 when the upgrade has been completed using a text editor edit 
/opt/vmware/var/lib/vami/update/data/info/manifest-installed.xml
and
/opt/vmware/share/htdocs/service/core/view-deploy.xml 
changing display name from 4.1 to 4.2

Examples of corrected view-deploy.xml 
     <property name="name" value="PowerChute Network Shutdown 4.2 for VMware"/>

Example of corrected manifest-installed.xml
  PowerChute Network Shutdown 4.2 for VMware
  4.2.0.6729
  4.2

 
Was this helpful?
What can we do to improve the information ?