CAMBODIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Air Economizers
Ecoflair Air Economizers
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
Module Optimized Cooling
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
Data Center Assessment Services
Install
Installation Services
Operate
Remote Monitoring Services
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
CAMBODIA - Choose Country or Region
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
No access to web agent using TLS 1.1 or TLS 1.2 with PowerChute Business Edition 9.0.1, 9.1.0, 9.0.2
Issue:
PowerChute Business Edition 9.0.1, 9.1.0 and 9.0.2 is packaged with JRE 6. JRE 6 is not compatible with TLS 1.1 or TLS 1.2
Product Line:
PowerChute Business Edition versions 9.0.1, 9.1.0 and 9.0.2
Environment:
OS: Linux, Solaris, Windows x64, x86
Cause:
JRE 6 is not compatible with TLS 1.1 or TLS 1.2 see the following for more info:
http://docs.oracle.com/javase/7/docs/technotes/guides/security/SunProviders.html
Solution:
Upgrade the version of JRE used by PowerChute to a version greater than 6
1
– Install a standalone x86 Java JRE (minimum JRE version 7)
Note:
On Linux, the RPM Package Manager installs the JRE to the /usr/java/ directory.
2
– Download the JRE Config Tool from the following location:
http://www.apc.com/tools/download/software_comp.cfm?sw_sku=SFPCBEJRE&id=125&swfam=125
3
– Run the JRE Config Tool to change the location of the Java JRE used by PowerChute to the JRE installed in step 1.