Technical FAQs

Ask a Question

Should the mounting rails of a sliding shelf be extended or retracted from the factory setting?

Issue:
Customers may want to retract or extend the rails of a sliding shelf.

Product Line:
NetShelter Sliding Shelves

Environment:
All versions and serial ranges.

Cause:
Rails may want to be extended or retracted to match where the rear mounting rails are installed.

Resolution:

The mounting rails of any sliding shelf should never be extended beyond the factory setting. Doing so will reduce the weight capacity of the sliding shelf.

Was this helpful?
What can we do to improve the information ?