Technical FAQs

Ask a Question

Is there a deeper version of the AR7711?

The PDU needs to be mounted deeper than AR7711 allows.

Product Line:
NetShelter SX

All versions and serial ranges.

The installation requires a deeper bracket.

There's not a deeper version of the AR7711, but two brackets can be combined to increase the depth of the furthest 0U mounting hole to approx. 5.7".
See attached file
Was this helpful?
What can we do to improve the information ?