CAMBODIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Air Economizers
Ecoflair Air Economizers
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
Module Optimized Cooling
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
Data Center Assessment Services
Install
Installation Services
Operate
Remote Monitoring Services
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
CAMBODIA - Choose Country or Region
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
Version 1 Appliance Will Not POST to NetBotz Central 2.x
Issue:
Version 1 Appliance Will Not POST to NetBotz Central 2.x
Product Line:
NetBotz
NetBotz Central
Environment:
NetBotz version 1
NetBotz Central 2.x
Cause:
Troubleshooting posting issues.
Resolution:
First, browse to the bot in question and check the PICPOSTURL field:
http://ip-of-wallbotz/http.txt
If the \""PICPOSTURL\"" doesn't have the port specified, it's the standard port 80, otherwise it should be whatever follows the hostname of the NBC.
If you want to change the port or the hostname/IP of the NBC, you’ll type the following in the URL field of the bot:
http://ip-of-wallbotz/setHttp?PICPOSTURL=http://ip-or-hostname-of-nbc-server:PORT/central/photoman
Note: If the ports are correct, and the hostname is correct, make sure the appliance can resolve the hostname of the NBC. To do this, telnet to the appliance and do a \""gethostbyname nbc-server-name\"".