Camera Motion Detection and Video Capture Overview - Version 2 Appliances
Issue:
Camera Motion Detection and Video Capture Overview - Version 2 Appliances
Product Line:
NetBotz
Environment:
NetBotz version 2 and 3
Cause:
All NetBotz Version 2 Appliances (320/420/500) support camera motion detection. It works by constantly taking pictures and capturing the current picture with the previous picture in its buffer. When motion is detected, then pictures are captured according to the Alert Capture Configuration for the camera:
Resolution:
When a camera captures pictures as a result of an alert / threshold, remember the following:
* Pictures are captured for a finite amount of time
* Once the defined amount of video is captured, no more video is captured until the alert condition clears and then starts again.