Are NetShelter SV cabinets compliant for seismic installation?
Issue:
The customer would like to know if the NetShelter SV cabinets are rated for seismic installations in UBC High Seismic Area or OSHPD.
Product Line:
NetShelter SV
Environment:
All versions and serial ranges
Cause:
A customer is looking for a seismic rated cabinet.
Resolution:
The NetShelter SV cabinets are not rated for seismic installation. There are no brackets or accessories that can make them compatible for a seismic installation.