Technical FAQs

Ask a Question

Video: How to turn On a Network Air FM Unit

Issue:
How to turn On a Network Air FM Unit.
 
Product line:
FM35-50, ACFM, IR40
 
Environment:
All Serial Numbers.
 
Cause:
Install, Operations.
 
Resolution:  

 

To turn on a Network Air FM unit through the display do the following procedure.
 
1 Press ESC key until you get to the main menu (On/Off Screen).
 
2 Press the ENTER key with the cursor pointed to the On/Off heading.
 
3 Press ENTER again and now you will be able to select either On or Off with the UP or DOWN arrows.
 
4 After you have made your selection press ENTER again and now the status led to the left of the display should be On if you selected ON or off if you selected OFF.
 
5 Press the ESC key until you get back to status screen.
 
 
Was this helpful?
What can we do to improve the information ?