What unit functions can I control through the web card of an ACSC1XX unit?
Issue:
What unit functions can I control through the web card of an ACSC1XX unit?
Product line:
ACSC1XX
Environment:
All Serial Numbers
Cause: FAQ
Resolution:
Unit configuration (operating mode, capacity mode, idle on leak) Temperature set points, unit delays, fan speed preference, alarm thresholds, configure alarm output, configure normal state
of contacts, assign service intervals, reset component run hours, display units (metric or English)
.