Large device discoveries in StruxureWare may affect performance.
Issue:
Discovering large numbers of nodes in StruxureWare Central or StruxureWare Data Center Expert can result in performance issues, sometimes requiring a system reboot.
Product Line:
StruxureWare Data Center Expert
StruxureWare Central
InfraStruxure Central
Environment:
All current versions
Cause:
Discoveries send larger amounts of data requests than normal scans. In many cases, other files such as configuration files and DDF files are also transferred during discovery
Resolution:
For best results, it is recommended that a large discovery job, for example 2000 SNMP devices, be run as several smaller discoveries.